EEO#.DIR

Description

Sets the direction of the emulated encoder output (EEO) with respect to the source feedback.

Value EEO#.MODE 0 EEO#.MODE 1 EEO#.MODE 2
0 (default) A leads B Positive rotation pulses CW Positive rotation DIR is not energized.
1 B leads A Positive rotation pulses CCW Positive rotation DIR is energized.

Examples

Code

This setting will reverse the direction of the EEO: if the source feedback is moving clockwise, the EEO will emulate a counter-clockwise movement.

-->EEO1.DIR

Context

For more information see Output - Encoder Emulation.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range 0 to 1
Default Value 0
Data Type Integer
See Also  
Stored in Non Volatile Memory Yes

Variants Supported

All variants are supported.